Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static StudioXformBuilder.PlanarizeMethodType |
StudioXformBuilder.PlanarizeMethodType.AT_PLANE_LOCATION
planarize at plane location
|
static StudioXformBuilder.PlanarizeMethodType |
StudioXformBuilder.PlanarizeMethodType.AT_POLE_LOCATION
planarize at pole location
|
static StudioXformBuilder.PlanarizeMethodType |
StudioXformBuilder.PlanarizeMethodType.ON_ABEST_FIT_PLANE
planarize at a best fit plane
|
Modifier and Type | Method and Description |
---|---|
StudioXformBuilder.PlanarizeMethodType |
StudioXformBuilder.planarizeMethod()
Deprecated.
Deprecated in NX8.5.0. Use
StudioXformBuilderEx instead.
|
static StudioXformBuilder.PlanarizeMethodType |
StudioXformBuilder.PlanarizeMethodType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static StudioXformBuilder.PlanarizeMethodType |
StudioXformBuilder.PlanarizeMethodType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static StudioXformBuilder.PlanarizeMethodType[] |
StudioXformBuilder.PlanarizeMethodType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
StudioXformBuilder.setPlanarizeMethod(StudioXformBuilder.PlanarizeMethodType planarizeMethod)
Deprecated.
Deprecated in NX8.5.0. Use
StudioXformBuilderEx instead.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.