Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static StudioXformBuilder.InsertKnotDirectionType |
StudioXformBuilder.InsertKnotDirectionType.UDIRECTION
Inser knot in U direction
|
static StudioXformBuilder.InsertKnotDirectionType |
StudioXformBuilder.InsertKnotDirectionType.VDIRECTION
Inser knot in V direction
|
Modifier and Type | Method and Description |
---|---|
StudioXformBuilder.InsertKnotDirectionType |
StudioXformBuilder.insertKnotDirection()
Deprecated.
Deprecated in NX8.5.0. Use
StudioXformBuilderEx instead.
|
static StudioXformBuilder.InsertKnotDirectionType |
StudioXformBuilder.InsertKnotDirectionType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static StudioXformBuilder.InsertKnotDirectionType |
StudioXformBuilder.InsertKnotDirectionType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static StudioXformBuilder.InsertKnotDirectionType[] |
StudioXformBuilder.InsertKnotDirectionType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
StudioXformBuilder.setInsertKnotDirection(StudioXformBuilder.InsertKnotDirectionType insertKnotDirection)
Deprecated.
Deprecated in NX8.5.0. Use
StudioXformBuilderEx instead.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.