Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static StudioSurfaceBuilder.TransitionOptions |
StudioSurfaceBuilder.TransitionOptions.CUBIC
Cubic
|
static StudioSurfaceBuilder.TransitionOptions |
StudioSurfaceBuilder.TransitionOptions.LINEAR_AND_BLEND
Linear and Blend
|
static StudioSurfaceBuilder.TransitionOptions |
StudioSurfaceBuilder.TransitionOptions.NO_END_CONSTRAINT
No End Constraint
|
static StudioSurfaceBuilder.TransitionOptions |
StudioSurfaceBuilder.TransitionOptions.NORMAL_TO_ALL_SECTIONS
Normal to All Sections
|
static StudioSurfaceBuilder.TransitionOptions |
StudioSurfaceBuilder.TransitionOptions.NORMAL_TO_END_SECTIONS
Normal to End Sections
|
Modifier and Type | Method and Description |
---|---|
StudioSurfaceBuilder.TransitionOptions |
StudioSurfaceBuilder.transition()
Returns the transition control
License requirements: features_modeling ("FEATURES MODELING"), nx_freeform_1 ("basic freeform modeling") . |
static StudioSurfaceBuilder.TransitionOptions |
StudioSurfaceBuilder.TransitionOptions.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static StudioSurfaceBuilder.TransitionOptions |
StudioSurfaceBuilder.TransitionOptions.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static StudioSurfaceBuilder.TransitionOptions[] |
StudioSurfaceBuilder.TransitionOptions.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
StudioSurfaceBuilder.setTransition(StudioSurfaceBuilder.TransitionOptions transition)
License requirements: features_modeling ("FEATURES MODELING"), nx_freeform_1 ("basic freeform modeling") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.