Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static StudioSplineBuilderEx.WCSOptionType |
StudioSplineBuilderEx.WCSOptionType.X
Along X axis
|
static StudioSplineBuilderEx.WCSOptionType |
StudioSplineBuilderEx.WCSOptionType.XY
In XY plane
|
static StudioSplineBuilderEx.WCSOptionType |
StudioSplineBuilderEx.WCSOptionType.XZ
In XZ plane
|
static StudioSplineBuilderEx.WCSOptionType |
StudioSplineBuilderEx.WCSOptionType.Y
Along Y axis
|
static StudioSplineBuilderEx.WCSOptionType |
StudioSplineBuilderEx.WCSOptionType.YZ
In YZ plane
|
static StudioSplineBuilderEx.WCSOptionType |
StudioSplineBuilderEx.WCSOptionType.Z
Along Z axis
|
Modifier and Type | Method and Description |
---|---|
static StudioSplineBuilderEx.WCSOptionType |
StudioSplineBuilderEx.WCSOptionType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static StudioSplineBuilderEx.WCSOptionType |
StudioSplineBuilderEx.WCSOptionType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static StudioSplineBuilderEx.WCSOptionType[] |
StudioSplineBuilderEx.WCSOptionType.values()
Returns an array that contains the values for this enum.
|
StudioSplineBuilderEx.WCSOptionType |
StudioSplineBuilderEx.wcsoption()
Returns the WCS option
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
void |
StudioSplineBuilderEx.setWCSOption(StudioSplineBuilderEx.WCSOptionType wcsOption)
License requirements: features_modeling ("FEATURES MODELING") OR cam_base ("CAM BASE") OR geometric_tol ("GDT") OR insp_programming ("INSPECTION PROGRAMMING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.