Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static StudioSplineBuilderEx.Types |
StudioSplineBuilderEx.Types.BY_POLES
Spline by poles
|
static StudioSplineBuilderEx.Types |
StudioSplineBuilderEx.Types.THROUGH_POINTS
Spline through points
|
Modifier and Type | Method and Description |
---|---|
StudioSplineBuilderEx.Types |
StudioSplineBuilderEx.type()
Returns the spline method
License requirements: None. |
static StudioSplineBuilderEx.Types |
StudioSplineBuilderEx.Types.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static StudioSplineBuilderEx.Types |
StudioSplineBuilderEx.Types.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static StudioSplineBuilderEx.Types[] |
StudioSplineBuilderEx.Types.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
StudioSplineBuilderEx.setType(StudioSplineBuilderEx.Types type)
License requirements: features_modeling ("FEATURES MODELING") OR cam_base ("CAM BASE") OR geometric_tol ("GDT") OR insp_programming ("INSPECTION PROGRAMMING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.