Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static StudioSplineBuilderEx.MovementMethodType |
StudioSplineBuilderEx.MovementMethodType.NORMAL
Movement along a face normal
|
static StudioSplineBuilderEx.MovementMethodType |
StudioSplineBuilderEx.MovementMethodType.PLANE
Movement in arbitrary plane
|
static StudioSplineBuilderEx.MovementMethodType |
StudioSplineBuilderEx.MovementMethodType.POLYGON
Movement along a relevant control polygon segment
|
static StudioSplineBuilderEx.MovementMethodType |
StudioSplineBuilderEx.MovementMethodType.VECTOR
Movement along arbitrary direction
|
static StudioSplineBuilderEx.MovementMethodType |
StudioSplineBuilderEx.MovementMethodType.VIEW
Movement in view plane
|
static StudioSplineBuilderEx.MovementMethodType |
StudioSplineBuilderEx.MovementMethodType.WCS
Movement along WCS principal axis or plane
|
Modifier and Type | Method and Description |
---|---|
StudioSplineBuilderEx.MovementMethodType |
StudioSplineBuilderEx.movementMethod()
Returns the movement method
License requirements: None. |
static StudioSplineBuilderEx.MovementMethodType |
StudioSplineBuilderEx.MovementMethodType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static StudioSplineBuilderEx.MovementMethodType |
StudioSplineBuilderEx.MovementMethodType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static StudioSplineBuilderEx.MovementMethodType[] |
StudioSplineBuilderEx.MovementMethodType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
StudioSplineBuilderEx.setMovementMethod(StudioSplineBuilderEx.MovementMethodType movementMethod)
License requirements: features_modeling ("FEATURES MODELING") OR cam_base ("CAM BASE") OR geometric_tol ("GDT") OR insp_programming ("INSPECTION PROGRAMMING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.