Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static StudioSplineBuilderEx.MatchKnotsTypes |
StudioSplineBuilderEx.MatchKnotsTypes.CUBIC
Match knots for cubic non-periodic spline
|
static StudioSplineBuilderEx.MatchKnotsTypes |
StudioSplineBuilderEx.MatchKnotsTypes.GENERAL
Match knots for general spline
|
static StudioSplineBuilderEx.MatchKnotsTypes |
StudioSplineBuilderEx.MatchKnotsTypes.NONE
No knot matching
|
Modifier and Type | Method and Description |
---|---|
StudioSplineBuilderEx.MatchKnotsTypes |
StudioSplineBuilderEx.matchKnotsType()
Returns a constraint to match knots at the defining points for a through point spline
License requirements: None. |
static StudioSplineBuilderEx.MatchKnotsTypes |
StudioSplineBuilderEx.MatchKnotsTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static StudioSplineBuilderEx.MatchKnotsTypes |
StudioSplineBuilderEx.MatchKnotsTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static StudioSplineBuilderEx.MatchKnotsTypes[] |
StudioSplineBuilderEx.MatchKnotsTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
StudioSplineBuilderEx.setMatchKnotsType(StudioSplineBuilderEx.MatchKnotsTypes matchKnotsType)
License requirements: features_modeling ("FEATURES MODELING") OR cam_base ("CAM BASE") OR geometric_tol ("GDT") OR insp_programming ("INSPECTION PROGRAMMING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.