Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static StudioSplineBuilder.Method |
StudioSplineBuilder.Method.BY_POLES
Spline by poles
|
static StudioSplineBuilder.Method |
StudioSplineBuilder.Method.THROUGH_POINTS
Spline through points
|
Modifier and Type | Method and Description |
---|---|
StudioSplineBuilder.Method |
StudioSplineBuilder.splineMethod()
Deprecated.
Deprecated in NX8.0.0. Use
StudioSplineBuilderEx instead.
|
static StudioSplineBuilder.Method |
StudioSplineBuilder.Method.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static StudioSplineBuilder.Method |
StudioSplineBuilder.Method.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static StudioSplineBuilder.Method[] |
StudioSplineBuilder.Method.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
StudioSplineBuilder.setNonParametricSpline(Spline spline,
StudioSplineBuilder.Method method)
Deprecated.
Deprecated in NX8.0.0. Use
StudioSplineBuilderEx instead.
|
void |
StudioSplineBuilder.setSplineMethod(StudioSplineBuilder.Method method)
Deprecated.
Deprecated in NX8.0.0. Use
StudioSplineBuilderEx instead.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.