Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static StepBuilder.StepWallMethods |
StepBuilder.StepWallMethods.BLEND
Blends the step-wall face
|
static StepBuilder.StepWallMethods |
StepBuilder.StepWallMethods.EXTENDTO_NEXT
Extends the wall face to intersect the next face
|
static StepBuilder.StepWallMethods |
StepBuilder.StepWallMethods.EXTENDTO_SELECTED
Extends the wall face to a selected face
|
static StepBuilder.StepWallMethods |
StepBuilder.StepWallMethods.NORMAL
Orients the step-wall face normal to the input face
|
static StepBuilder.StepWallMethods |
StepBuilder.StepWallMethods.OFFSETOF_STEP_FACE
Makes the step-wall face offset from the step face
|
static StepBuilder.StepWallMethods |
StepBuilder.StepWallMethods.RULED_RAMP
Replaces the step-wall face with a ruled ramp face
|
static StepBuilder.StepWallMethods |
StepBuilder.StepWallMethods.VARIABLE_OFFSET_RAMP
Replaces the step-wall face with a variable offset ramp face
|
Modifier and Type | Method and Description |
---|---|
StepBuilder.StepWallMethods |
StepBuilder.stepWallMethod1()
Returns the step wall method 1
License requirements: None. |
StepBuilder.StepWallMethods |
StepBuilder.stepWallMethod2()
Returns the step wall method 2
License requirements: None. |
static StepBuilder.StepWallMethods |
StepBuilder.StepWallMethods.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static StepBuilder.StepWallMethods |
StepBuilder.StepWallMethods.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static StepBuilder.StepWallMethods[] |
StepBuilder.StepWallMethods.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
StepBuilder.setStepWallMethod1(StepBuilder.StepWallMethods stepWallMethod1)
License requirements: nx_aero_design (" NX Aero Design") . |
void |
StepBuilder.setStepWallMethod2(StepBuilder.StepWallMethods stepWallMethod2)
License requirements: nx_aero_design (" NX Aero Design") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.