Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static StepBuilder.StepTypes |
StepBuilder.StepTypes.CHAMFER
Adds a step at the edge of a face similar to a chamfer
|
static StepBuilder.StepTypes |
StepBuilder.StepTypes.END
Adds a step from a boundary to the edge of a face.
|
static StepBuilder.StepTypes |
StepBuilder.StepTypes.MIDDLE
Adds a step between two boundary curves
|
Modifier and Type | Method and Description |
---|---|
StepBuilder.StepTypes |
StepBuilder.stepType()
Returns the step type
License requirements: None. |
static StepBuilder.StepTypes |
StepBuilder.StepTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static StepBuilder.StepTypes |
StepBuilder.StepTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static StepBuilder.StepTypes[] |
StepBuilder.StepTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
StepBuilder.setStepType(StepBuilder.StepTypes stepType)
License requirements: nx_aero_design (" NX Aero Design") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.