Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static StepBuilder.DepthMethods |
StepBuilder.DepthMethods.OFFSET_FACE
Offsets the motion face to produce a step
|
static StepBuilder.DepthMethods |
StepBuilder.DepthMethods.TO_SELECTED
Replaces the motion face with a selected face to produce a step
|
Modifier and Type | Method and Description |
---|---|
StepBuilder.DepthMethods |
StepBuilder.depthMethod()
Returns the selected step depth method
License requirements: None. |
static StepBuilder.DepthMethods |
StepBuilder.DepthMethods.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static StepBuilder.DepthMethods |
StepBuilder.DepthMethods.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static StepBuilder.DepthMethods[] |
StepBuilder.DepthMethods.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
StepBuilder.setDepthMethod(StepBuilder.DepthMethods depthMethod)
License requirements: nx_aero_design (" NX Aero Design") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.