Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static SpineCurveBuilder.ArcSegmentsTypes |
SpineCurveBuilder.ArcSegmentsTypes.SIMPLE |
static SpineCurveBuilder.ArcSegmentsTypes |
SpineCurveBuilder.ArcSegmentsTypes.SMOOTH |
Modifier and Type | Method and Description |
---|---|
SpineCurveBuilder.ArcSegmentsTypes |
SpineCurveBuilder.arcSegmentsType()
Returns the option indicating type of shape
License requirements: None. |
static SpineCurveBuilder.ArcSegmentsTypes |
SpineCurveBuilder.ArcSegmentsTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SpineCurveBuilder.ArcSegmentsTypes |
SpineCurveBuilder.ArcSegmentsTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SpineCurveBuilder.ArcSegmentsTypes[] |
SpineCurveBuilder.ArcSegmentsTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
SpineCurveBuilder.setArcSegmentsType(SpineCurveBuilder.ArcSegmentsTypes curveOption)
License requirements: solid_modeling ("SOLIDS MODELING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.