Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static SnipSurfaceBuilder.Types |
SnipSurfaceBuilder.Types.ISOPARAM_SNIP |
static SnipSurfaceBuilder.Types |
SnipSurfaceBuilder.Types.SNIP_AT_PLANE |
static SnipSurfaceBuilder.Types |
SnipSurfaceBuilder.Types.SNIP_CURVE |
static SnipSurfaceBuilder.Types |
SnipSurfaceBuilder.Types.SNIP_SURFACE |
Modifier and Type | Method and Description |
---|---|
SnipSurfaceBuilder.Types |
SnipSurfaceBuilder.type()
Returns the snipping method accessor
License requirements: None. |
static SnipSurfaceBuilder.Types |
SnipSurfaceBuilder.Types.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SnipSurfaceBuilder.Types |
SnipSurfaceBuilder.Types.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SnipSurfaceBuilder.Types[] |
SnipSurfaceBuilder.Types.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
SnipSurfaceBuilder.setType(SnipSurfaceBuilder.Types type)
License requirements: None. |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.