Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Method and Description |
---|---|
SmoothRangeBuilder |
SmoothRangeBuilderList.findItem(int index)
Returns the object at the input index.
|
SmoothRangeBuilder[] |
SmoothRangeBuilderList.getContents()
Gets the contents of the entire list
License requirements: None. |
SmoothRangeBuilder |
FlowBlendBuilder.newSmoothRange()
The smooth range object's create function
License requirements: solid_modeling ("SOLIDS MODELING") . |
Modifier and Type | Method and Description |
---|---|
void |
SmoothRangeBuilderList.append(SmoothRangeBuilder object)
Appends an object to the list
License requirements: None. |
void |
SmoothRangeBuilderList.append(SmoothRangeBuilder[] objects)
Appends a set of objects to the list
License requirements: None. |
void |
SmoothRangeBuilderList.erase(SmoothRangeBuilder obj)
Erases the object from the list, but does not delete the object.
|
void |
SmoothRangeBuilderList.erase(SmoothRangeBuilder obj,
ObjectList.DeleteOption deleteOption)
Erases the object from the list.
|
int |
SmoothRangeBuilderList.findIndex(SmoothRangeBuilder obj)
Finds the index where the input object appears.
|
void |
SmoothRangeBuilderList.insert(int location,
SmoothRangeBuilder object)
Inserts an object at the specified location
License requirements: None. |
void |
SmoothRangeBuilderList.setContents(SmoothRangeBuilder[] objects)
Sets the contents of the entire list.
|
void |
SmoothRangeBuilderList.swap(SmoothRangeBuilder object1,
SmoothRangeBuilder object2)
Exchanges the position of two objects inside the list.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.