Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static SmoothCurveStringBuilder.Types |
SmoothCurveStringBuilder.Types.CURVES_ON_SURFACES |
static SmoothCurveStringBuilder.Types |
SmoothCurveStringBuilder.Types.FREE_CURVES |
Modifier and Type | Method and Description |
---|---|
SmoothCurveStringBuilder.Types |
SmoothCurveStringBuilder.type()
Returns the type of input curves whether free or on surface.
|
static SmoothCurveStringBuilder.Types |
SmoothCurveStringBuilder.Types.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SmoothCurveStringBuilder.Types |
SmoothCurveStringBuilder.Types.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SmoothCurveStringBuilder.Types[] |
SmoothCurveStringBuilder.Types.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
SmoothCurveStringBuilder.setType(SmoothCurveStringBuilder.Types type)
License requirements: studio_free_form ("STUDIO FREE FORM") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.