Package | Description |
---|---|
nxopen.features.sheetmetal |
Provides classes and interfaces for Sheet Metal Features.
|
Modifier and Type | Method and Description |
---|---|
SketchFeature |
LoftedFlangeBuilder.endSketch()
Returns the end section sketch as slave.
|
SketchFeature |
TabBuilder.sketch()
Returns the sketch of tab
License requirements: nx_sheet_metal ("NX Sheet Metal") OR nx_flexible_pcb ("NX Flexible PCB") . |
SketchFeature |
NormalCutoutBuilder.sketch()
Returns the internal sketch used by the normal cutout, if it exists.
|
SketchFeature |
LouverBuilder.sketch()
Returns the internal sketch used by the louver's section.
|
SketchFeature |
LighteningCutoutBuilder.sketch()
Returns the Sketch used by Lightening Cutout
License requirements: None. |
SketchFeature |
JogBuilder.sketch()
Returns
License requirements: nx_sheet_metal ("NX Sheet Metal") OR nx_flexible_pcb ("NX Flexible PCB") . |
SketchFeature |
EdgeRipBuilder.sketch()
Returns the Slave Sketch used by the Edge Rip, If one exists.
|
SketchFeature |
DrawnCutoutBuilder.sketch()
Returns the Slave Sketch used by the Drawn Cutout, If one exists.
|
SketchFeature |
DimpleBuilder.sketch()
Returns the Slave Sketch used by the Dimple, If one exists.
|
SketchFeature |
ConvertToSheetmetalBuilder.sketch()
Returns the internal sketch (used to specify rip curves), if it exists.
|
SketchFeature |
ContourFlangeBuilder.sketch()
Returns the sketch
License requirements: nx_sheet_metal ("NX Sheet Metal") OR nx_flexible_pcb ("NX Flexible PCB") . |
SketchFeature |
BendBuilder.sketch()
Returns the Sketch
License requirements: nx_sheet_metal ("NX Sheet Metal") OR nx_flexible_pcb ("NX Flexible PCB") . |
SketchFeature |
BeadBuilder.sketch()
Returns the Slave Sketch used by the Bead, If one exists.
|
SketchFeature |
LoftedFlangeBuilder.startSketch()
Returns the start section sketch as slave.
|
Modifier and Type | Method and Description |
---|---|
void |
LoftedFlangeBuilder.setEndSketch(SketchFeature slaveEndSketch)
Sets the end section sketch as slave.
|
void |
TabBuilder.setSketch(SketchFeature sketch)
Sets the sketch of tab
License requirements: nx_sheet_metal ("NX Sheet Metal") OR nx_flexible_pcb ("NX Flexible PCB") . |
void |
NormalCutoutBuilder.setSketch(SketchFeature sketch)
Sets the internal sketch used by the normal cutout, if it exists.
|
void |
LouverBuilder.setSketch(SketchFeature sketch)
Sets the internal sketch used by the louver's section.
|
void |
JogBuilder.setSketch(SketchFeature sketch)
License requirements: nx_sheet_metal ("NX Sheet Metal") OR nx_flexible_pcb ("NX Flexible PCB") . |
void |
EdgeRipBuilder.setSketch(SketchFeature sketch)
Sets the Slave Sketch used by the Edge Rip, If one exists.
|
void |
DrawnCutoutBuilder.setSketch(SketchFeature sketch)
Sets the Slave Sketch used by the Drawn Cutout, If one exists.
|
void |
DimpleBuilder.setSketch(SketchFeature sketch)
Sets the Slave Sketch used by the Dimple, If one exists.
|
void |
ConvertToSheetmetalBuilder.setSketch(SketchFeature sketch)
Sets the internal sketch (used to specify rip curves), if it exists.
|
void |
ContourFlangeBuilder.setSketch(SketchFeature sketch)
Sets the sketch
License requirements: nx_sheet_metal ("NX Sheet Metal") OR nx_flexible_pcb ("NX Flexible PCB") . |
void |
BendBuilder.setSketch(SketchFeature sketch)
Sets the Sketch
License requirements: nx_sheet_metal ("NX Sheet Metal") OR nx_flexible_pcb ("NX Flexible PCB") . |
void |
BeadBuilder.setSketch(SketchFeature sketch)
Sets the Slave Sketch used by the Bead, If one exists.
|
void |
LoftedFlangeBuilder.setStartSketch(SketchFeature slaveStartSketch)
Sets the start section sketch as slave.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.