Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static SketchConversionStatus.Type |
SketchConversionStatus.Type.FAILURE
Convert to sketch failed
|
static SketchConversionStatus.Type |
SketchConversionStatus.Type.PARTIAL_SUCCESS
Convert to sketch succeeded with reason/issues
|
static SketchConversionStatus.Type |
SketchConversionStatus.Type.SUCCESS
Convert to sketch successful
|
Modifier and Type | Method and Description |
---|---|
SketchConversionStatus.Type |
SketchConversionStatus.status()
Returns the status of conversion of a feature to an independent sketch.
|
static SketchConversionStatus.Type |
SketchConversionStatus.Type.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SketchConversionStatus.Type |
SketchConversionStatus.Type.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SketchConversionStatus.Type[] |
SketchConversionStatus.Type.values()
Returns an array that contains the values for this enum.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.