Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static ShelfBuilder.ReferenceType |
ShelfBuilder.ReferenceType.CURVE |
static ShelfBuilder.ReferenceType |
ShelfBuilder.ReferenceType.DATUM_PLANE |
static ShelfBuilder.ReferenceType |
ShelfBuilder.ReferenceType.FACE |
static ShelfBuilder.ReferenceType |
ShelfBuilder.ReferenceType.POINT |
Modifier and Type | Method and Description |
---|---|
ShelfBuilder.ReferenceType |
ShelfBuilder.refType1()
Returns the ref type1
License requirements: None. |
ShelfBuilder.ReferenceType |
ShelfBuilder.refType2()
Returns the ref type2
License requirements: None. |
static ShelfBuilder.ReferenceType |
ShelfBuilder.ReferenceType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ShelfBuilder.ReferenceType |
ShelfBuilder.ReferenceType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ShelfBuilder.ReferenceType[] |
ShelfBuilder.ReferenceType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
ShelfBuilder.setRefType1(ShelfBuilder.ReferenceType refType1)
License requirements: nx_aero_design (" NX Aero Design") . |
void |
ShelfBuilder.setRefType2(ShelfBuilder.ReferenceType refType2)
License requirements: nx_aero_design (" NX Aero Design") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.