Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static ShelfBuilder.LengthMethods |
ShelfBuilder.LengthMethods.FULL |
static ShelfBuilder.LengthMethods |
ShelfBuilder.LengthMethods.SHELF_FROM_END |
static ShelfBuilder.LengthMethods |
ShelfBuilder.LengthMethods.STEP_FROM_END |
static ShelfBuilder.LengthMethods |
ShelfBuilder.LengthMethods.TO_SELECTED |
Modifier and Type | Method and Description |
---|---|
ShelfBuilder.LengthMethods |
ShelfBuilder.lengthMethod()
Returns the length method
License requirements: None. |
static ShelfBuilder.LengthMethods |
ShelfBuilder.LengthMethods.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ShelfBuilder.LengthMethods |
ShelfBuilder.LengthMethods.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ShelfBuilder.LengthMethods[] |
ShelfBuilder.LengthMethods.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
ShelfBuilder.setLengthMethod(ShelfBuilder.LengthMethods lengthMethod)
License requirements: nx_aero_design (" NX Aero Design") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.