Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static SectionSurfaceBuilderEx.SpineStartFlowType |
SectionSurfaceBuilderEx.SpineStartFlowType.ISO_LINE_U
flow direction follows iso u of the start surface
|
static SectionSurfaceBuilderEx.SpineStartFlowType |
SectionSurfaceBuilderEx.SpineStartFlowType.ISO_LINE_V
flow direction follows iso v of the start surface
|
static SectionSurfaceBuilderEx.SpineStartFlowType |
SectionSurfaceBuilderEx.SpineStartFlowType.NOT_SPECIFIED
flow direction not specified
|
static SectionSurfaceBuilderEx.SpineStartFlowType |
SectionSurfaceBuilderEx.SpineStartFlowType.PERPENDICULAR
flow direction perpendicular to the guide
|
Modifier and Type | Method and Description |
---|---|
SectionSurfaceBuilderEx.SpineStartFlowType |
SectionSurfaceBuilderEx.spineStartFlowDirection()
Returns the spine start flow direction.
|
static SectionSurfaceBuilderEx.SpineStartFlowType |
SectionSurfaceBuilderEx.SpineStartFlowType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SectionSurfaceBuilderEx.SpineStartFlowType |
SectionSurfaceBuilderEx.SpineStartFlowType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SectionSurfaceBuilderEx.SpineStartFlowType[] |
SectionSurfaceBuilderEx.SpineStartFlowType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
SectionSurfaceBuilderEx.setSpineStartFlowDirection(SectionSurfaceBuilderEx.SpineStartFlowType spineStartFlowDirection)
License requirements: nx_freeform_2 ("advanced freeform modeling") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.