Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static SectionSurfaceBuilderEx.SpineEndFlowType |
SectionSurfaceBuilderEx.SpineEndFlowType.ISO_LINE_U
flow direction follows iso u of the start surface
|
static SectionSurfaceBuilderEx.SpineEndFlowType |
SectionSurfaceBuilderEx.SpineEndFlowType.ISO_LINE_V
flow direction follows iso v of the start surface
|
static SectionSurfaceBuilderEx.SpineEndFlowType |
SectionSurfaceBuilderEx.SpineEndFlowType.NOT_SPECIFIED
flow direction not specified
|
static SectionSurfaceBuilderEx.SpineEndFlowType |
SectionSurfaceBuilderEx.SpineEndFlowType.PERPENDICULAR
flow direction perpendicular to the guide
|
Modifier and Type | Method and Description |
---|---|
SectionSurfaceBuilderEx.SpineEndFlowType |
SectionSurfaceBuilderEx.spineEndFlowDirection()
Returns the spine end flow direction.
|
static SectionSurfaceBuilderEx.SpineEndFlowType |
SectionSurfaceBuilderEx.SpineEndFlowType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SectionSurfaceBuilderEx.SpineEndFlowType |
SectionSurfaceBuilderEx.SpineEndFlowType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SectionSurfaceBuilderEx.SpineEndFlowType[] |
SectionSurfaceBuilderEx.SpineEndFlowType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
SectionSurfaceBuilderEx.setSpineEndFlowDirection(SectionSurfaceBuilderEx.SpineEndFlowType spineEndFlowDirection)
License requirements: nx_freeform_2 ("advanced freeform modeling") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.