Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static SectionSurfaceBuilderEx.SectionMethodFilletBridgeType |
SectionSurfaceBuilderEx.SectionMethodFilletBridgeType.CONTINUITY
continuity options
|
static SectionSurfaceBuilderEx.SectionMethodFilletBridgeType |
SectionSurfaceBuilderEx.SectionMethodFilletBridgeType.INHERIT_SHAPE
inherit shape option
|
Modifier and Type | Method and Description |
---|---|
SectionSurfaceBuilderEx.SectionMethodFilletBridgeType |
SectionSurfaceBuilderEx.sectionMethodFilletBridge()
Returns the section method fillet bridge.
|
static SectionSurfaceBuilderEx.SectionMethodFilletBridgeType |
SectionSurfaceBuilderEx.SectionMethodFilletBridgeType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SectionSurfaceBuilderEx.SectionMethodFilletBridgeType |
SectionSurfaceBuilderEx.SectionMethodFilletBridgeType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SectionSurfaceBuilderEx.SectionMethodFilletBridgeType[] |
SectionSurfaceBuilderEx.SectionMethodFilletBridgeType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
SectionSurfaceBuilderEx.setSectionMethodFilletBridge(SectionSurfaceBuilderEx.SectionMethodFilletBridgeType sectionMethodFilletBridge)
License requirements: nx_freeform_2 ("advanced freeform modeling") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.