Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static SectionSurfaceBuilderEx.LinearType |
SectionSurfaceBuilderEx.LinearType.POINT_ANGLE
Point Angle mode
|
static SectionSurfaceBuilderEx.LinearType |
SectionSurfaceBuilderEx.LinearType.TANGENT_TANGENT
Tangent Tangent mode
|
Modifier and Type | Method and Description |
---|---|
SectionSurfaceBuilderEx.LinearType |
SectionSurfaceBuilderEx.linearTypeMode()
Returns the linear type mode.
|
static SectionSurfaceBuilderEx.LinearType |
SectionSurfaceBuilderEx.LinearType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SectionSurfaceBuilderEx.LinearType |
SectionSurfaceBuilderEx.LinearType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SectionSurfaceBuilderEx.LinearType[] |
SectionSurfaceBuilderEx.LinearType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
SectionSurfaceBuilderEx.setLinearTypeMode(SectionSurfaceBuilderEx.LinearType linearTypeMode)
License requirements: nx_freeform_2 ("advanced freeform modeling") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.