Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static SectionSurfaceBuilderEx.ControlRegionType |
SectionSurfaceBuilderEx.ControlRegionType.END
depth and skew applied to the end section of the section surface
|
static SectionSurfaceBuilderEx.ControlRegionType |
SectionSurfaceBuilderEx.ControlRegionType.ENTIRE
depth and skew applied to the entire section surface
|
static SectionSurfaceBuilderEx.ControlRegionType |
SectionSurfaceBuilderEx.ControlRegionType.START
depth and skew applied to the start section of the section surface
|
Modifier and Type | Method and Description |
---|---|
SectionSurfaceBuilderEx.ControlRegionType |
SectionSurfaceBuilderEx.controlRegion()
Returns the control region.
|
static SectionSurfaceBuilderEx.ControlRegionType |
SectionSurfaceBuilderEx.ControlRegionType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SectionSurfaceBuilderEx.ControlRegionType |
SectionSurfaceBuilderEx.ControlRegionType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SectionSurfaceBuilderEx.ControlRegionType[] |
SectionSurfaceBuilderEx.ControlRegionType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
SectionSurfaceBuilderEx.setControlRegion(SectionSurfaceBuilderEx.ControlRegionType controlRegion)
License requirements: nx_freeform_2 ("advanced freeform modeling") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.