Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static SectionSurfaceBuilder.SectionMethodCircularTangentEnum |
SectionSurfaceBuilder.SectionMethodCircularTangentEnum.COVER_ARC
cover arc
|
static SectionSurfaceBuilder.SectionMethodCircularTangentEnum |
SectionSurfaceBuilder.SectionMethodCircularTangentEnum.FILLET_ARC
fillet arc
|
Modifier and Type | Method and Description |
---|---|
SectionSurfaceBuilder.SectionMethodCircularTangentEnum |
SectionSurfaceBuilder.sectionMethodCircularTangent()
Deprecated.
Deprecated in NX9.0.0. Use
SectionSurfaceBuilderEx instead.
|
static SectionSurfaceBuilder.SectionMethodCircularTangentEnum |
SectionSurfaceBuilder.SectionMethodCircularTangentEnum.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SectionSurfaceBuilder.SectionMethodCircularTangentEnum |
SectionSurfaceBuilder.SectionMethodCircularTangentEnum.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SectionSurfaceBuilder.SectionMethodCircularTangentEnum[] |
SectionSurfaceBuilder.SectionMethodCircularTangentEnum.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
SectionSurfaceBuilder.setSectionMethodCircularTangent(SectionSurfaceBuilder.SectionMethodCircularTangentEnum sectionMethodCircularTangent)
Deprecated.
Deprecated in NX9.0.0. Use
SectionSurfaceBuilderEx instead.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.