Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static ScaleCurveBuilder.ScaleCurveType |
ScaleCurveBuilder.ScaleCurveType.NON_UNIFORM
NonUniform scaling
|
static ScaleCurveBuilder.ScaleCurveType |
ScaleCurveBuilder.ScaleCurveType.UNIFORM
Uniform scaling
|
Modifier and Type | Method and Description |
---|---|
ScaleCurveBuilder.ScaleCurveType |
ScaleCurveBuilder.scaleType()
Returns the scale type
License requirements: None. |
static ScaleCurveBuilder.ScaleCurveType |
ScaleCurveBuilder.ScaleCurveType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ScaleCurveBuilder.ScaleCurveType |
ScaleCurveBuilder.ScaleCurveType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ScaleCurveBuilder.ScaleCurveType[] |
ScaleCurveBuilder.ScaleCurveType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
ScaleCurveBuilder.setScaleType(ScaleCurveBuilder.ScaleCurveType scaleType)
License requirements: solid_modeling ("SOLIDS MODELING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.