Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static RibBuilder.RibDraftOptions |
RibBuilder.RibDraftOptions.FROM_CAP
Draft from cap
|
static RibBuilder.RibDraftOptions |
RibBuilder.RibDraftOptions.NONE
No Draft
|
Modifier and Type | Method and Description |
---|---|
RibBuilder.RibDraftOptions |
RibBuilder.ribDraftOption()
Returns the rib draft options
License requirements: None. |
static RibBuilder.RibDraftOptions |
RibBuilder.RibDraftOptions.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static RibBuilder.RibDraftOptions |
RibBuilder.RibDraftOptions.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static RibBuilder.RibDraftOptions[] |
RibBuilder.RibDraftOptions.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
RibBuilder.setRibDraftOption(RibBuilder.RibDraftOptions ribDraftOption)
License requirements: solid_modeling ("SOLIDS MODELING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.