Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static ResizeCurveBuilder.ValueType |
ResizeCurveBuilder.ValueType.DIAMETER |
static ResizeCurveBuilder.ValueType |
ResizeCurveBuilder.ValueType.RADIUS |
Modifier and Type | Method and Description |
---|---|
static ResizeCurveBuilder.ValueType |
ResizeCurveBuilder.ValueType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ResizeCurveBuilder.ValueType |
ResizeCurveBuilder.ValueType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
ResizeCurveBuilder.ValueType |
ResizeCurveBuilder.valueOption()
Returns the size option
License requirements: None. |
static ResizeCurveBuilder.ValueType[] |
ResizeCurveBuilder.ValueType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
ResizeCurveBuilder.setValueOption(ResizeCurveBuilder.ValueType valueOption)
License requirements: solid_modeling ("SOLIDS MODELING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.