Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static ReplaceFeatureBuilder.MappingMethodType |
ReplaceFeatureBuilder.MappingMethodType.MAP_ALL_OBJECTS
Not supported yet
|
static ReplaceFeatureBuilder.MappingMethodType |
ReplaceFeatureBuilder.MappingMethodType.MAP_ONLY_OBJECTS_WITH_MODELING_DEPENDENCIES |
Modifier and Type | Method and Description |
---|---|
ReplaceFeatureBuilder.MappingMethodType |
ReplaceFeatureBuilder.mappingMethod()
Returns the mapping method
License requirements: None. |
static ReplaceFeatureBuilder.MappingMethodType |
ReplaceFeatureBuilder.MappingMethodType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ReplaceFeatureBuilder.MappingMethodType |
ReplaceFeatureBuilder.MappingMethodType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ReplaceFeatureBuilder.MappingMethodType[] |
ReplaceFeatureBuilder.MappingMethodType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
ReplaceFeatureBuilder.setMappingMethod(ReplaceFeatureBuilder.MappingMethodType mappingMethod)
License requirements: None. |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.