Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Method and Description |
---|---|
RegionListItemBuilder |
VarOffsetFaceBuilder.createRegionListItem()
The region selection type dim object's create function
License requirements: None. |
RegionListItemBuilder |
RegionListItemBuilderList.findItem(int index)
Returns the object at the input index.
|
RegionListItemBuilder[] |
RegionListItemBuilderList.getContents()
Gets the contents of the entire list
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
void |
RegionListItemBuilderList.append(RegionListItemBuilder object)
Appends an object to the list
License requirements: None. |
void |
RegionListItemBuilderList.append(RegionListItemBuilder[] objects)
Appends a set of objects to the list
License requirements: None. |
void |
RegionListItemBuilderList.erase(RegionListItemBuilder obj)
Erases the object from the list, but does not delete the object.
|
void |
RegionListItemBuilderList.erase(RegionListItemBuilder obj,
ObjectList.DeleteOption deleteOption)
Erases the object from the list.
|
int |
RegionListItemBuilderList.findIndex(RegionListItemBuilder obj)
Finds the index where the input object appears.
|
void |
RegionListItemBuilderList.insert(int location,
RegionListItemBuilder object)
Inserts an object at the specified location
License requirements: None. |
void |
RegionListItemBuilderList.setContents(RegionListItemBuilder[] objects)
Sets the contents of the entire list.
|
void |
RegionListItemBuilderList.swap(RegionListItemBuilder object1,
RegionListItemBuilder object2)
Exchanges the position of two objects inside the list.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.