Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static RapidSurfaceBuilder.AttachmentTypes |
RapidSurfaceBuilder.AttachmentTypes.FACET_BODY
attach to facet body
|
static RapidSurfaceBuilder.AttachmentTypes |
RapidSurfaceBuilder.AttachmentTypes.NONE
attach to nothing
|
Modifier and Type | Method and Description |
---|---|
RapidSurfaceBuilder.AttachmentTypes |
RapidSurfaceBuilder.attachmentType()
Returns the attachment type
License requirements: studio_free_form ("STUDIO FREE FORM") . |
static RapidSurfaceBuilder.AttachmentTypes |
RapidSurfaceBuilder.AttachmentTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static RapidSurfaceBuilder.AttachmentTypes |
RapidSurfaceBuilder.AttachmentTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static RapidSurfaceBuilder.AttachmentTypes[] |
RapidSurfaceBuilder.AttachmentTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
RapidSurfaceBuilder.setAttachmentType(RapidSurfaceBuilder.AttachmentTypes option)
License requirements: studio_free_form ("STUDIO FREE FORM") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.