Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static ProjectCurveBuilder.ProjectionOptionType |
ProjectCurveBuilder.ProjectionOptionType.EQUAL_ARC_LENGTH
Represents Equal Arc Length
|
static ProjectCurveBuilder.ProjectionOptionType |
ProjectCurveBuilder.ProjectionOptionType.NONE
Represents None
|
static ProjectCurveBuilder.ProjectionOptionType |
ProjectCurveBuilder.ProjectionOptionType.PROJECT_BOTH_SIDES
Represents Project Both Sides
|
Modifier and Type | Method and Description |
---|---|
ProjectCurveBuilder.ProjectionOptionType |
ProjectCurveBuilder.projectionOption()
Returns the projection option type
License requirements: None. |
static ProjectCurveBuilder.ProjectionOptionType |
ProjectCurveBuilder.ProjectionOptionType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ProjectCurveBuilder.ProjectionOptionType |
ProjectCurveBuilder.ProjectionOptionType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ProjectCurveBuilder.ProjectionOptionType[] |
ProjectCurveBuilder.ProjectionOptionType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
ProjectCurveBuilder.setProjectionOption(ProjectCurveBuilder.ProjectionOptionType projectionOption)
License requirements: solid_modeling ("SOLIDS MODELING") OR cam_base ("CAM BASE") OR insp_programming ("INSPECTION PROGRAMMING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.