Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static ProjectCurveBuilder.ArcLengthType |
ProjectCurveBuilder.ArcLengthType.BOTH_XY
Represents Both X and Y
|
static ProjectCurveBuilder.ArcLengthType |
ProjectCurveBuilder.ArcLengthType.FIRST_XTHEN_Y
Represents First X then Y
|
static ProjectCurveBuilder.ArcLengthType |
ProjectCurveBuilder.ArcLengthType.FIRST_YTHEN_X
Represents First Y then X
|
static ProjectCurveBuilder.ArcLengthType |
ProjectCurveBuilder.ArcLengthType.XONLY
Represents X only
|
static ProjectCurveBuilder.ArcLengthType |
ProjectCurveBuilder.ArcLengthType.YONLY
Represents Y only
|
Modifier and Type | Method and Description |
---|---|
ProjectCurveBuilder.ArcLengthType |
ProjectCurveBuilder.equalArcLengthMethod()
Returns the equal arc length method
License requirements: None. |
static ProjectCurveBuilder.ArcLengthType |
ProjectCurveBuilder.ArcLengthType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ProjectCurveBuilder.ArcLengthType |
ProjectCurveBuilder.ArcLengthType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ProjectCurveBuilder.ArcLengthType[] |
ProjectCurveBuilder.ArcLengthType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
ProjectCurveBuilder.setEqualArcLengthMethod(ProjectCurveBuilder.ArcLengthType arcLengthMethod)
License requirements: solid_modeling ("SOLIDS MODELING") OR cam_base ("CAM BASE") OR insp_programming ("INSPECTION PROGRAMMING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.