Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Method and Description |
---|---|
PointSetFacePercentageBuilder |
PointSetBuilder.createFacePercentageListItem()
Create an entry for the face percentage list.
|
PointSetFacePercentageBuilder |
PointSetFacePercentageBuilderList.findItem(int index)
Returns the object at the input index.
|
PointSetFacePercentageBuilder[] |
PointSetFacePercentageBuilderList.getContents()
Gets the contents of the entire list
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
void |
PointSetFacePercentageBuilderList.append(PointSetFacePercentageBuilder object)
Appends an object to the list
License requirements: None. |
void |
PointSetFacePercentageBuilderList.append(PointSetFacePercentageBuilder[] objects)
Appends a set of objects to the list
License requirements: None. |
void |
PointSetFacePercentageBuilderList.erase(PointSetFacePercentageBuilder obj)
Erases the object from the list, but does not delete the object.
|
void |
PointSetFacePercentageBuilderList.erase(PointSetFacePercentageBuilder obj,
ObjectList.DeleteOption deleteOption)
Erases the object from the list.
|
int |
PointSetFacePercentageBuilderList.findIndex(PointSetFacePercentageBuilder obj)
Finds the index where the input object appears.
|
void |
PointSetFacePercentageBuilderList.insert(int location,
PointSetFacePercentageBuilder object)
Inserts an object at the specified location
License requirements: None. |
void |
PointSetFacePercentageBuilderList.setContents(PointSetFacePercentageBuilder[] objects)
Sets the contents of the entire list.
|
void |
PointSetFacePercentageBuilderList.swap(PointSetFacePercentageBuilder object1,
PointSetFacePercentageBuilder object2)
Exchanges the position of two objects inside the list.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.