Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static PointSetBuilder.Types |
PointSetBuilder.Types.CURVE_POINTS
Create points along curve.
|
static PointSetBuilder.Types |
PointSetBuilder.Types.FACE_POINTS
Create points on face
|
static PointSetBuilder.Types |
PointSetBuilder.Types.INTERSECTION_POINTS
Create intersection points
|
static PointSetBuilder.Types |
PointSetBuilder.Types.SPLINE_POINTS
Create points along spline.
|
Modifier and Type | Method and Description |
---|---|
PointSetBuilder.Types |
PointSetBuilder.type()
Returns the type setting.
|
static PointSetBuilder.Types |
PointSetBuilder.Types.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static PointSetBuilder.Types |
PointSetBuilder.Types.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static PointSetBuilder.Types[] |
PointSetBuilder.Types.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
PointSetBuilder.setType(PointSetBuilder.Types type)
License requirements: solid_modeling ("SOLIDS MODELING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.