Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static PointSetBuilder.FacePointsType |
PointSetBuilder.FacePointsType.BSURFACE_POLES
Points will be created at surface poles.
|
static PointSetBuilder.FacePointsType |
PointSetBuilder.FacePointsType.FACE_PERCENTAGE
A point will be created at given face percentages.
|
static PointSetBuilder.FacePointsType |
PointSetBuilder.FacePointsType.PATTERN
Points will be created based on a defined pattern.
|
Modifier and Type | Method and Description |
---|---|
PointSetBuilder.FacePointsType |
PointSetBuilder.facePointsBy()
Returns the face points definition setting.
|
static PointSetBuilder.FacePointsType |
PointSetBuilder.FacePointsType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static PointSetBuilder.FacePointsType |
PointSetBuilder.FacePointsType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static PointSetBuilder.FacePointsType[] |
PointSetBuilder.FacePointsType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
PointSetBuilder.setFacePointsBy(PointSetBuilder.FacePointsType facePointsBy)
License requirements: solid_modeling ("SOLIDS MODELING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.