Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static PatternFeatureBuilder.OutputOptions |
PatternFeatureBuilder.OutputOptions.COPIES_OF_INPUT_FEATURES
Copies of Input features
|
static PatternFeatureBuilder.OutputOptions |
PatternFeatureBuilder.OutputOptions.COPIES_OF_INPUT_FEATURES_IN_GROUP
Copies of Input features in Group
|
static PatternFeatureBuilder.OutputOptions |
PatternFeatureBuilder.OutputOptions.PATTERN_FEATURE
Pattern Feature
|
Modifier and Type | Method and Description |
---|---|
PatternFeatureBuilder.OutputOptions |
PatternFeatureBuilder.outputOption()
Returns the output option
License requirements: None. |
static PatternFeatureBuilder.OutputOptions |
PatternFeatureBuilder.OutputOptions.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static PatternFeatureBuilder.OutputOptions |
PatternFeatureBuilder.OutputOptions.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static PatternFeatureBuilder.OutputOptions[] |
PatternFeatureBuilder.OutputOptions.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
PatternFeatureBuilder.setOutputOption(PatternFeatureBuilder.OutputOptions outputOption)
License requirements: solid_modeling ("SOLIDS MODELING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.