Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Method and Description |
---|---|
PartGeometryCopySelectBuilder |
PartGeometryCopyBuilder.createSelectionBuilder(PartGeometryCopyBuilder.Type objectType)
Creates a part geometry copy select builder
License requirements: None. |
PartGeometryCopySelectBuilder |
PartGeometryCopySelectBuilderList.findItem(int index)
Returns the object at the input index.
|
PartGeometryCopySelectBuilder[] |
PartGeometryCopySelectBuilderList.getContents()
Gets the contents of the entire list
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
void |
PartGeometryCopySelectBuilderList.append(PartGeometryCopySelectBuilder object)
Appends an object to the list
License requirements: None. |
void |
PartGeometryCopySelectBuilderList.append(PartGeometryCopySelectBuilder[] objects)
Appends a set of objects to the list
License requirements: None. |
void |
PartGeometryCopySelectBuilderList.erase(PartGeometryCopySelectBuilder obj)
Erases the object from the list, but does not delete the object.
|
void |
PartGeometryCopySelectBuilderList.erase(PartGeometryCopySelectBuilder obj,
ObjectList.DeleteOption deleteOption)
Erases the object from the list.
|
int |
PartGeometryCopySelectBuilderList.findIndex(PartGeometryCopySelectBuilder obj)
Finds the index where the input object appears.
|
void |
PartGeometryCopySelectBuilderList.insert(int location,
PartGeometryCopySelectBuilder object)
Inserts an object at the specified location
License requirements: None. |
void |
PartGeometryCopySelectBuilderList.setContents(PartGeometryCopySelectBuilder[] objects)
Sets the contents of the entire list.
|
void |
PartGeometryCopySelectBuilderList.swap(PartGeometryCopySelectBuilder object1,
PartGeometryCopySelectBuilder object2)
Exchanges the position of two objects inside the list.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.