Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static OffsetSurfaceBuilder.OutputOptionType |
OffsetSurfaceBuilder.OutputOptionType.ONE_FEATURE_FOR_ALL_FACES |
static OffsetSurfaceBuilder.OutputOptionType |
OffsetSurfaceBuilder.OutputOptionType.ONE_FEATURE_FOR_CONNECTED_FACES |
static OffsetSurfaceBuilder.OutputOptionType |
OffsetSurfaceBuilder.OutputOptionType.ONE_FEATURE_FOR_EACH_FACE |
Modifier and Type | Method and Description |
---|---|
OffsetSurfaceBuilder.OutputOptionType |
OffsetSurfaceBuilder.outputOption()
Returns the offset surface output option based on the enum
OffsetSurfaceBuilder.OutputOptionType
License requirements: None. |
static OffsetSurfaceBuilder.OutputOptionType |
OffsetSurfaceBuilder.OutputOptionType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static OffsetSurfaceBuilder.OutputOptionType |
OffsetSurfaceBuilder.OutputOptionType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static OffsetSurfaceBuilder.OutputOptionType[] |
OffsetSurfaceBuilder.OutputOptionType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
OffsetSurfaceBuilder.setOutputOption(OffsetSurfaceBuilder.OutputOptionType outputOption)
License requirements: solid_modeling ("SOLIDS MODELING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.