Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static OffsetSurfaceBuilder.OrientationMethodType |
OffsetSurfaceBuilder.OrientationMethodType.SPECIFY_INTERIOR_POSITION |
static OffsetSurfaceBuilder.OrientationMethodType |
OffsetSurfaceBuilder.OrientationMethodType.USE_EXISTING_NORMALS |
Modifier and Type | Method and Description |
---|---|
OffsetSurfaceBuilder.OrientationMethodType |
OffsetSurfaceBuilder.getOrientationMethod()
Returns the offset surface orientation method based on the
OffsetSurfaceBuilder.OutputOptionType
License requirements: None. |
static OffsetSurfaceBuilder.OrientationMethodType |
OffsetSurfaceBuilder.OrientationMethodType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static OffsetSurfaceBuilder.OrientationMethodType |
OffsetSurfaceBuilder.OrientationMethodType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static OffsetSurfaceBuilder.OrientationMethodType[] |
OffsetSurfaceBuilder.OrientationMethodType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
OffsetSurfaceBuilder.setOrientationMethod(OffsetSurfaceBuilder.OrientationMethodType orientationMethod)
Sets the orientation method
License requirements: solid_modeling ("SOLIDS MODELING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.