Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static NSidedSurfaceBuilder.SurfaceType |
NSidedSurfaceBuilder.SurfaceType.TRIANGULAR_PATCH
Triangular Patch
|
static NSidedSurfaceBuilder.SurfaceType |
NSidedSurfaceBuilder.SurfaceType.TRIMMED_PATCH
Trimmed Patch
|
Modifier and Type | Method and Description |
---|---|
NSidedSurfaceBuilder.SurfaceType |
NSidedSurfaceBuilder.type()
Returns the surface type
License requirements: features_modeling ("FEATURES MODELING"), nx_freeform_1 ("basic freeform modeling") . |
static NSidedSurfaceBuilder.SurfaceType |
NSidedSurfaceBuilder.SurfaceType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static NSidedSurfaceBuilder.SurfaceType |
NSidedSurfaceBuilder.SurfaceType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static NSidedSurfaceBuilder.SurfaceType[] |
NSidedSurfaceBuilder.SurfaceType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
NSidedSurfaceBuilder.setType(NSidedSurfaceBuilder.SurfaceType surfaceType)
License requirements: features_modeling ("FEATURES MODELING"), nx_freeform_1 ("basic freeform modeling") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.