Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static NSidedSurfaceBuilder.FlowDirectionType |
NSidedSurfaceBuilder.FlowDirectionType.ADJACENT_EDGES
adjacent edges
|
static NSidedSurfaceBuilder.FlowDirectionType |
NSidedSurfaceBuilder.FlowDirectionType.ISO_UVLINE
uv line
|
static NSidedSurfaceBuilder.FlowDirectionType |
NSidedSurfaceBuilder.FlowDirectionType.NOT_SPECIFIED
not specified
|
static NSidedSurfaceBuilder.FlowDirectionType |
NSidedSurfaceBuilder.FlowDirectionType.PERPENDICULAR
perpendicular
|
Modifier and Type | Method and Description |
---|---|
NSidedSurfaceBuilder.FlowDirectionType |
NSidedSurfaceBuilder.flowDirection()
Returns the flow direction
License requirements: features_modeling ("FEATURES MODELING"), nx_freeform_1 ("basic freeform modeling") . |
static NSidedSurfaceBuilder.FlowDirectionType |
NSidedSurfaceBuilder.FlowDirectionType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static NSidedSurfaceBuilder.FlowDirectionType |
NSidedSurfaceBuilder.FlowDirectionType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static NSidedSurfaceBuilder.FlowDirectionType[] |
NSidedSurfaceBuilder.FlowDirectionType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
NSidedSurfaceBuilder.setFlowDirection(NSidedSurfaceBuilder.FlowDirectionType button)
License requirements: features_modeling ("FEATURES MODELING"), nx_freeform_1 ("basic freeform modeling") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.