Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static MoveFaceBuilder.Types |
MoveFaceBuilder.Types.ROTATE_ABOUT_AXIS
Move faces by rotating about an axis
|
static MoveFaceBuilder.Types |
MoveFaceBuilder.Types.ROTATE_BETWEEN_TWO_AXES
Move faces by rotating the axis from the first to the second
|
static MoveFaceBuilder.Types |
MoveFaceBuilder.Types.TRANSLATE_BETWEEN_TWO_POINTS
Move faces in the direction and distance defined by the two points
|
static MoveFaceBuilder.Types |
MoveFaceBuilder.Types.TRANSLATE_DIRECTION_AND_DISTANCE
Direction and Distance for moving the faces
|
Modifier and Type | Method and Description |
---|---|
MoveFaceBuilder.Types |
MoveFaceBuilder.type()
Returns the type, don't use it until nx502
License requirements: None. |
static MoveFaceBuilder.Types |
MoveFaceBuilder.Types.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static MoveFaceBuilder.Types |
MoveFaceBuilder.Types.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static MoveFaceBuilder.Types[] |
MoveFaceBuilder.Types.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
MoveFaceBuilder.setType(MoveFaceBuilder.Types moveType)
License requirements: solid_modeling ("SOLIDS MODELING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.