Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static MirrorFeatureBuilder.PlaneOptions |
MirrorFeatureBuilder.PlaneOptions.EXISTING
existing plane
|
static MirrorFeatureBuilder.PlaneOptions |
MirrorFeatureBuilder.PlaneOptions.NEW
new plane
|
Modifier and Type | Method and Description |
---|---|
MirrorFeatureBuilder.PlaneOptions |
MirrorFeatureBuilder.planeOption()
Returns the plane option
License requirements: None. |
static MirrorFeatureBuilder.PlaneOptions |
MirrorFeatureBuilder.PlaneOptions.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static MirrorFeatureBuilder.PlaneOptions |
MirrorFeatureBuilder.PlaneOptions.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static MirrorFeatureBuilder.PlaneOptions[] |
MirrorFeatureBuilder.PlaneOptions.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
MirrorFeatureBuilder.setPlaneOption(MirrorFeatureBuilder.PlaneOptions planeOptions)
License requirements: solid_modeling ("SOLIDS MODELING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.