Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static MirrorBodyBuilder.FeatureOptionType |
MirrorBodyBuilder.FeatureOptionType.ONE_FEATURE_FOR_ALL_BODIES
An option to create one mirror or linked mirror body feature for all selected bodies as body collector
|
static MirrorBodyBuilder.FeatureOptionType |
MirrorBodyBuilder.FeatureOptionType.SEPARATE_FEATURE_FOR_EACH_BODY
An option to create a separate mirror or linked mirror body feature per single body
|
Modifier and Type | Method and Description |
---|---|
MirrorBodyBuilder.FeatureOptionType |
MirrorBodyBuilder.featureOption()
Returns the feature option type
License requirements: None. |
static MirrorBodyBuilder.FeatureOptionType |
MirrorBodyBuilder.FeatureOptionType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static MirrorBodyBuilder.FeatureOptionType |
MirrorBodyBuilder.FeatureOptionType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static MirrorBodyBuilder.FeatureOptionType[] |
MirrorBodyBuilder.FeatureOptionType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
MirrorBodyBuilder.setFeatureOption(MirrorBodyBuilder.FeatureOptionType featureOptionType)
License requirements: solid_modeling ("SOLIDS MODELING") OR cam_base ("CAM BASE") OR insp_programming ("INSPECTION PROGRAMMING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.