Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static MidSurfaceByFacePairsBuilder.TrimmingOptionType |
MidSurfaceByFacePairsBuilder.TrimmingOptionType.ADVANCED_TRIMMING
Advanced trimming
|
static MidSurfaceByFacePairsBuilder.TrimmingOptionType |
MidSurfaceByFacePairsBuilder.TrimmingOptionType.BODY_BASED_TRIMMING
Body based trimming
|
static MidSurfaceByFacePairsBuilder.TrimmingOptionType |
MidSurfaceByFacePairsBuilder.TrimmingOptionType.SKIP_TRIMMING
Skip trimming for replacement sheets
|
static MidSurfaceByFacePairsBuilder.TrimmingOptionType |
MidSurfaceByFacePairsBuilder.TrimmingOptionType.TRIMTO_SIDE1WITH_NO_EXTENSION
Trim to master
|
Modifier and Type | Method and Description |
---|---|
MidSurfaceByFacePairsBuilder.TrimmingOptionType |
MidSurfaceByFacePairsBuilder.trimmingOption()
Returns the trimming option
License requirements: None. |
static MidSurfaceByFacePairsBuilder.TrimmingOptionType |
MidSurfaceByFacePairsBuilder.TrimmingOptionType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static MidSurfaceByFacePairsBuilder.TrimmingOptionType |
MidSurfaceByFacePairsBuilder.TrimmingOptionType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static MidSurfaceByFacePairsBuilder.TrimmingOptionType[] |
MidSurfaceByFacePairsBuilder.TrimmingOptionType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
MidSurfaceByFacePairsBuilder.setTrimmingOption(MidSurfaceByFacePairsBuilder.TrimmingOptionType trimmingOption)
License requirements: solid_modeling ("SOLIDS MODELING") . |
void |
MidSurfaceByFacePairsBuilder.trim(MidSurfaceByFacePairsBuilder.TrimmingOptionType trimmingOption,
NXObject[] facePairs)
Trim the face pairs
License requirements: solid_modeling ("SOLIDS MODELING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.