Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static MidSurfaceByFacePairsBuilder.SurfaceType |
MidSurfaceByFacePairsBuilder.SurfaceType.CLOUD_OF_POINTS
Cloud of points
|
static MidSurfaceByFacePairsBuilder.SurfaceType |
MidSurfaceByFacePairsBuilder.SurfaceType.LARGE
Use single largest surface
|
static MidSurfaceByFacePairsBuilder.SurfaceType |
MidSurfaceByFacePairsBuilder.SurfaceType.OFFSET
Use offset
|
static MidSurfaceByFacePairsBuilder.SurfaceType |
MidSurfaceByFacePairsBuilder.SurfaceType.SIDE1
Use side 1 faces as mid sheet
|
static MidSurfaceByFacePairsBuilder.SurfaceType |
MidSurfaceByFacePairsBuilder.SurfaceType.STANDARD
Default surface creation method
|
Modifier and Type | Method and Description |
---|---|
static MidSurfaceByFacePairsBuilder.SurfaceType |
MidSurfaceByFacePairsBuilder.SurfaceType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static MidSurfaceByFacePairsBuilder.SurfaceType |
MidSurfaceByFacePairsBuilder.SurfaceType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static MidSurfaceByFacePairsBuilder.SurfaceType[] |
MidSurfaceByFacePairsBuilder.SurfaceType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
MidSurfaceByFacePairsBuilder.modifyMidsurface(MidSurfaceByFacePairsBuilder.SurfaceType surfaceOption,
NXObject[] facePairs)
Use cloud of points to generate neutral sheet
License requirements: solid_modeling ("SOLIDS MODELING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.