Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static MeshTransformerBuilder.SmoothingType |
MeshTransformerBuilder.SmoothingType.HIGH
Smoothing high
|
static MeshTransformerBuilder.SmoothingType |
MeshTransformerBuilder.SmoothingType.LOW
Smoothing low
|
static MeshTransformerBuilder.SmoothingType |
MeshTransformerBuilder.SmoothingType.NORMAL
Smoothing normal
|
static MeshTransformerBuilder.SmoothingType |
MeshTransformerBuilder.SmoothingType.VERY_HIGH
Smoothing high
|
static MeshTransformerBuilder.SmoothingType |
MeshTransformerBuilder.SmoothingType.VERY_LOW
Smoothing very low
|
Modifier and Type | Method and Description |
---|---|
MeshTransformerBuilder.SmoothingType |
MeshTransformerBuilder.smoothingOption()
Returns the smoothing option used in the transformation or morphing calculations
License requirements: None. |
static MeshTransformerBuilder.SmoothingType |
MeshTransformerBuilder.SmoothingType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static MeshTransformerBuilder.SmoothingType |
MeshTransformerBuilder.SmoothingType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static MeshTransformerBuilder.SmoothingType[] |
MeshTransformerBuilder.SmoothingType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
MeshTransformerBuilder.setSmoothingOption(MeshTransformerBuilder.SmoothingType smoothingOption)
License requirements: None. |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.