Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static MeshTransformerBuilder.ContinuityType |
MeshTransformerBuilder.ContinuityType.C2
C2 continuity
|
static MeshTransformerBuilder.ContinuityType |
MeshTransformerBuilder.ContinuityType.C4
C4 continuity
|
Modifier and Type | Method and Description |
---|---|
MeshTransformerBuilder.ContinuityType |
MeshTransformerBuilder.continuityTypeOption()
Returns the continuity type option
License requirements: None. |
static MeshTransformerBuilder.ContinuityType |
MeshTransformerBuilder.ContinuityType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static MeshTransformerBuilder.ContinuityType |
MeshTransformerBuilder.ContinuityType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static MeshTransformerBuilder.ContinuityType[] |
MeshTransformerBuilder.ContinuityType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
MeshTransformerBuilder.setContinuityTypeOption(MeshTransformerBuilder.ContinuityType continuityTypeOption)
License requirements: None. |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.