Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static MathIntegrationBuilder.LocationTypes |
MathIntegrationBuilder.LocationTypes.EMBEDDED
Worksheet is embedded in part.
|
static MathIntegrationBuilder.LocationTypes |
MathIntegrationBuilder.LocationTypes.OPERATING_SYSTEM
Worksheet is on the native OS file system.
|
static MathIntegrationBuilder.LocationTypes |
MathIntegrationBuilder.LocationTypes.TEAMCENTER
Worksheet is in Teamcenter.
|
Modifier and Type | Method and Description |
---|---|
MathIntegrationBuilder.LocationTypes |
MathIntegrationBuilder.location()
Returns the source location of the Symbolica or Maple worksheet.
|
static MathIntegrationBuilder.LocationTypes |
MathIntegrationBuilder.LocationTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static MathIntegrationBuilder.LocationTypes |
MathIntegrationBuilder.LocationTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static MathIntegrationBuilder.LocationTypes[] |
MathIntegrationBuilder.LocationTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
MathIntegrationBuilder.setLocation(MathIntegrationBuilder.LocationTypes location)
License requirements: solid_modeling ("SOLIDS MODELING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.